AXIS#.GEAR.FBSOURCE

Description

This parameter is the gearing master source.

Examples

Usage

The gearing master source can be any of the position feedbacks supported by the drive. AXIS#.GEAR.FBSOURCE should be set to the feedback device ID.

Code

This example demonstrates setting the gearing master source to FB3 on the X23 connector. For example, this feedback input could be used for A/B quadrature, step and direction, or CW/CCW pulse signals.

--> AXIS1.GEAR.FBSOURCE 3

Context

For more information see Electronic Gearing.

The following image shows where this keyword is used in WorkBench.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range

0 – None

1 – FB1 (X1 Connector)

2 – FB2 (X2 Connector)

3 – FB3 (X23 Connector)

4 – FB4 (X21 Connector)

5 – FB5 (X22 Connector)

Default Value 0
Data Type Integer
See Also AXIS#.CMDSOURCE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.GEAR.FBSOURCE

5006h

06h

Unsigned8

-

-

Read/Write

No

AXIS2.GEAR.FBSOURCE

5106h

06h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.GEAR.FBSOURCE

5505

1581

Unsigned8

Read/Write

-

AXIS2.GEAR.FBSOURCE

71041

1158

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.GEAR.FBSOURCE

5505

Unsigned8

Read/Write

-